Why my sja1105Q can not switch any packages?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why my sja1105Q can not switch any packages?

287件の閲覧回数
BravoEven
Contributor I

Hi NXP:

      I have put the demo configuration in sja1105QS_simple.py ## into my SJA1105QEL via SPI interface, andthe register 01h is 0x80000... which shows that the configuration has completed. But when I put the switch between the net interface on the wall and my PC , my PC cannot connect to the internet. Is there any more configuration needed? Hardware layout is shown below:codecodecodecodeHArdwareHArdware

MPC574xB/C/G and SJA1105P/Q/R/S Gateway Evaluation Kit | NXP Semiconductors the code is from SJA1105X_CONFIG-GENTOOL in the link upon.

Thanks! Sincerely!

0 件の賞賛
返信
0 返答(返信)