UART2 Tx and Rx Pins are not pulling down to "0"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART2 Tx and Rx Pins are not pulling down to "0"

252 次查看
Suresh123
Contributor I

Hi Team

I have designed im8mp custom board. While debugging through UART2 the Tx and Rx pins are not pulling down during the debug as in EVK because of this I am getting the prints on the terminal but unable to stop at UBOOT. The processor is able to receive the signal but unable to respond.

 

With Regards,

Suresh Gondi

0 项奖励
回复
1 回复

222 次查看
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @Suresh123 

 

It appears a device tree issue. Please refer to:

imx8mp-evk.dts - chosen

imx8mp-evk.dts - uart2 node

imx8mp-evk.dts - pinctrl

 

You can refer to IMX8MPLUS  software because you are using the same UART for CORTEX-A debug.

 

Best reagrds.

 

Salas.

0 项奖励
回复