Dear
We are developing with TJA1057, and we are looking for SPEC as follows. 1.Differential output slew rate : 20V/us(Min), 40V/us(Max)
2. Nominal BIT time: 2000ns (CAN Speed: 500kbps)
3. CAN H, L input voltage deviation (Dominant): 0.9~2.0~5.0V
Please check how to record.
Thank you
BR
sorry.,,,
We need to find the answer to the question and enter it into the customer's request table.
Thank
All of the TJA1057 electrical parameters showed in page8-10. Static characteristics of datasheet, except that we don't have other more.
What do you mean record? test?