TJA1057

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1057

402 Views
michaellee1
Contributor I

 

Dear 

 

We are developing with TJA1057, and we are looking for SPEC as follows. 1.Differential output slew rate : 20V/us(Min), 40V/us(Max)

2. Nominal BIT time: 2000ns (CAN Speed: 500kbps)

3. CAN H, L input voltage deviation (Dominant): 0.9~2.0~5.0V

 

Please check how to record.

Thank you

BR

Tags (1)
0 Kudos
Reply
3 Replies

396 Views
michaellee1
Contributor I

sorry.,,,

We need to find the answer to the question and enter it into the customer's request table.

Thank 

0 Kudos
Reply

389 Views
guoweisun
NXP TechSupport
NXP TechSupport

All of the TJA1057 electrical parameters showed in page8-10. Static characteristics of datasheet, except that we don't have other more.

0 Kudos
Reply

397 Views
guoweisun
NXP TechSupport
NXP TechSupport

What do you mean record? test?

 

0 Kudos
Reply