Dear
We are developing with TJA1057, and we are looking for SPEC as follows. 1.Differential output slew rate : 20V/us(Min), 40V/us(Max)
2. Nominal BIT time: 2000ns (CAN Speed: 500kbps)
3. CAN H, L input voltage deviation (Dominant): 0.9~2.0~5.0V
Please check how to record.
Thank you
BR
sorry.,,,
We need to find the answer to the question and enter it into the customer's request table.
Thank