TJA1040 can总线如何变为显性?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1040 can总线如何变为显性?

289 Views
lsy23
Contributor I

我用5V给TJA1040供电,STB与TXD都接GND,测量CANH、CANL却为2.5V(隐性);请问STB与TXD怎样接才能使CANH、CANL为显性呢?

0 Kudos
Reply
1 Reply

282 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Lee,

please pull the STB pin low (to GND) to set the TJA1040 to normal mode.

JozefKozon_0-1669635954280.png

 

Then, by pulling the TXD pin low, the CANH and CANL pins will be set to recessive state. 

JozefKozon_1-1669635954543.png

 

JozefKozon_2-1669635954554.png

 

If you want to put the CANH and CANL pins to dominant state, please pull the TXD pin to high state. Minimally above 2V, maximally to VCC+0.3V. The TXD pins has an internal pull-up to the VCC pin. Leaving the TXD pin floating, should also set the CANH and CANL pins to dominant state.

JozefKozon_3-1669635954688.png

 

JozefKozon_4-1669635954980.png

 

With Best Regards,

Jozef

0 Kudos
Reply