. ./fsl-setup-env -m t2080rdb-64b
Configuring for t2080rdb-64b ...
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b’: Permission denied
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/sstate-cache’: Permission denied
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b’: Permission denied
Error: The builddir (/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b) does not exist!
ERROR: the local.conf is not created, Exit ...
It can not mkdir as a non-root
but It also can't execute this command as a root
Does anyone have this problem? give me a favor
Thank you !
Please install QorIQ SDK 2.0 with non-root account.
Please go to folder /home/can/QorIQ-SDK-V2.0-20160527-yocto/ and check whether you can execute the following command.
$ mkdir build_t2080rdb-64b