Set Up Poky first step

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set Up Poky first step

617 Views
zmq001
Contributor I

. ./fsl-setup-env -m t2080rdb-64b
Configuring for t2080rdb-64b ...
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b’: Permission denied
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/sstate-cache’: Permission denied
mkdir: cannot create directory ‘/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b’: Permission denied
Error: The builddir (/home/can/QorIQ-SDK-V2.0-20160527-yocto/build_t2080rdb-64b) does not exist!
ERROR: the local.conf is not created, Exit ...

It can not mkdir as a non-root

but It also can't execute this command as a root 

Does anyone have this problem? give me a favor

Thank you !

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

609 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please install QorIQ SDK 2.0 with non-root account.

Please go to folder /home/can/QorIQ-SDK-V2.0-20160527-yocto/ and check whether you can execute the following command.

$ mkdir build_t2080rdb-64b

0 Kudos
Reply