Hi! I want to set a SGTL5000 into an inactive state. My idea is to remove the power supply to do so. But which one? There are three of them: VDDA, VDDIO and VDDD. Do I have to switch off all of them or only one(or two?).
The background is: The SGTL5000 is part of an audio solution which is sometimes exposed to severe EMC troubles which cannot be fixed. I have very often the situation that the SGTLs ADC is out of order and is just producing digital zeros then. Sometimes the SGTL is not responding at all anymore. So my idea is: Switch the power off/on to perform a reset.
Hello,
In this case I do recommend to perform some test switching VDDA.
Please note that VDDD and VDDA are the main supplies of the device. Therefore, it might work but you should perform some tests before.
Regards,
David
Hello,
I hope all is great with you.
You are correct, unfortunately the SGTL500 device does not have a reset pin.
In this case, the preferred supply sequencing is VDDIO/VDDA (it does not matter which comes first) and then VDDD. So, I do recommend to perform some tests using the VDDIO/VDDA supply rails.
I hope this information helps.
Regards,
David