SC18IM704 UART message rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IM704 UART message rate

175 Views
Tix00
Contributor II

Hi to everyone! wich is the maximum message rate (I2C transactions) for this IC?

Tags (2)
0 Kudos
2 Replies

150 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vicent,

The I2C clock rate is configurable via I2CClkL and I2CClkH registers and can be set up to 375 kHz.

Capture.JPG

BR, Tomas

0 Kudos

147 Views
Tix00
Contributor II

Hi Tomas, thanks for your fast reply.

Your table referes to I2C bus clock frequency, but my question is about the overall IC capacity for processing UART messages to the I2C machine. I mean to send a simple (two bytes) SxxxxxxP I2C write [not waiting for an answer] command message to the UART interface and dump it to the I2C bus.

Thank you in advance!

0 Kudos