Hi,there:
Now, I want use hse function in A53-Linux, but when i append hse to yocto'confuration file according "S32G3_LinuxBSP_38.0_User_Manual.pdf , Chapter 10 " , I modified and append "build_s32g399ardb3/conf/local.config" like below:
DISTRO_FEATURES:append = " hse"
NXP_FIRMWARE_LOCAL_DIR = " /home/chao/s32g3" /* Here, I placed the hse package and modefied the package's name to HSE_FW_S32G3XX_0_2_16_1 */
DISTRO_FEATURES:append = " secboot"
HSE_LIC = "license.rtf"
HSE_VERSION = "0_2_16_1"
HSE_SOC_REV = "rev1.1"
HSE_LIC_MD5 = " ??? " /* I'm not sure where can i get this Md5 Signature */
Execute : bitbake fsl-image-auto , thne lots of errors occures,
can anyone tell me how to build and use the hse function in the a53-linux ?
Hello, @wenyunhao
Thanks for the feedback.
Hope it helps.
Best Regards
Chenyin
Hello, @wenyunhao
Thanks for the question.
You may set it referencing the following:
DISTRO_FEATURES:append = " hse"
NXP_FIRMWARE_LOCAL_DIR = "/home/test/hse"
Hope it helps.
Best Regards
Chenyin
hi, thanks for your replay:
Mabye you didn't understand my question, I want to use HSE' reversion is "0.2.26.1" not the default " 0_2_22_0" , accroding the user manual, how can I get the HSE_LIC_MD5 ' value ?