S32DS新建例程出现大量错误

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS新建例程出现大量错误

2,180件の閲覧回数
duxingchenchn
Contributor I

用S32DS新建例程时,会出现很多错误。会有一些头文件显示不存在,然后大部分错误也是变量不存在,请问是什么问题。批注 2020-03-17 145136.png

タグ(1)
0 件の賞賛
返信
5 返答(返信)

1,961件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

did you generate PE code before building the project?

Use menu Project->Generate Processor Expert Code or click the icon on Component window.

BR, Petr

0 件の賞賛
返信

1,961件の閲覧回数
duxingchenchn
Contributor I

hi,

i found that problem, but  after generating PE code,

there was still a error: 

Ld error: cannot run program"": Launching failed C/C++ problem

i tried to reinstall S32DS, but there was an error: online license can not be deleted.

how to delete it?

thx

vic

0 件の賞賛
返信

1,961件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

not sure of teh error, can you share full log from S32DS?

BTW, tehre is new S32DS version 2.2. You can try to use that; https://community.nxp.com/docs/DOC-345517 

BR, Petr

0 件の賞賛
返信

1,961件の閲覧回数
18362881285
Contributor II

我也遇到了同样问题,后来发现是例程里面的generation文件夹里面的文件不能生成。我解决的办法是新添加PE,把报错的PE都添加进去。他们这个例程不知道是什么原因

0 件の賞賛
返信

1,961件の閲覧回数
duxingchenchn
Contributor I

你好,能留个联系方式吗,我重装了,还是不行,你的最后解决了吗?

0 件の賞賛
返信