RTC time changing to default values after some time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC time changing to default values after some time

1,637件の閲覧回数
pnaven03
Contributor I

Hi Team,

Am using raspberry pi  board , interface with RTC , setting the hardware clock using "hwclock --set" command , reading the clock using hwclock -r command, initially reading properly as a set time but after some time changing to default time values..

Thanks in advance,

Nv.

0 件の賞賛
返信
3 返答(返信)

1,413件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Naveen,

What RTC device are you using? I can help you with its configuration. Can you share your schematic?

Regards,

David

0 件の賞賛
返信

1,413件の閲覧回数
pnaven03
Contributor I

Hi David,

We are using rtc-pcf8563 device and driver registered successfully ,

Initially clock , date setting and reading properly ,

after one day time changed to one hour delay , There is kernel logs for

debug. Please can you help me.

Please check once attachment.

Regards,

Naveen Kumar,

0 件の賞賛
返信

1,413件の閲覧回数
vinodmaverickr0
Contributor IV

Hi Naveen,


This is nxp community. So I think you should ask this question in raspberry community (for better support). BTW you can also get the assistance here if you will elaborate your question (like which RTC module are you using  and if it is on the I2C so you can check the i2c communication through i2c utility) in a precise way.

Thanks,

Vinod

0 件の賞賛
返信