Questions about the KW45B41Z83AFPAR 「BOOT_CONFIG」 pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about the KW45B41Z83AFPAR 「BOOT_CONFIG」 pin

ソリューションへジャンプ
744件の閲覧回数
kkobayashi1
Contributor I

For the 「KW45B41Z83AFPAR」, the 「BOOT_CONFIG」 pin is set to Hi at BOOT, but do you need an external pulldown during normal operation?

0 件の賞賛
返信
1 解決策
669件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kkobayashi1 ,

 

We believe that if the BOOT_CONFIG pin is left open (not connected to a defined logic level), it will likely float and transition between high and low voltage levels unpredictably.

So, it should better pull-up or pull-down definitely. 

 

Best regards,

Gavin

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
703件の閲覧回数
kkobayashi1
Contributor I

Thank you for your reply.

If the BOOT _ CONFIG pin is Open, will it recognize "H" or "L" at startup?

0 件の賞賛
返信
670件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kkobayashi1 ,

 

We believe that if the BOOT_CONFIG pin is left open (not connected to a defined logic level), it will likely float and transition between high and low voltage levels unpredictably.

So, it should better pull-up or pull-down definitely. 

 

Best regards,

Gavin

0 件の賞賛
返信
725件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kkobayashi1 ,

Thanks for contacting NXP support.

After the board boots, we should keep the [BOOT_CONFIG] pin unchanged, no external pull-down is required.

 

Best regards,

Gavin

0 件の賞賛
返信