Hello Flavio Caruso,
I guess you maybe need a programmer for production.
Maybe you can use PEMicro U-Cyclone (Fx), pls refer:
PEmicro | Experts in Embedded tools for Flash Programming and Development
You can query all device supported from the following link:
PEmicro | Experts in Embedded tools for Flash Programming and Development
It doesn't include MWCT1013, but the PC software for U-Cyclone can support it. Pls update your PC software if there is no PN MWCT1013 in your PC software.
Hello Flavio Caruso,
I guess you maybe need a programmer for production.
Maybe you can use PEMicro U-Cyclone (Fx), pls refer:
PEmicro | Experts in Embedded tools for Flash Programming and Development
You can query all device supported from the following link:
PEmicro | Experts in Embedded tools for Flash Programming and Development
It doesn't include MWCT1013, but the PC software for U-Cyclone can support it. Pls update your PC software if there is no PN MWCT1013 in your PC software.
Hi Flavio,
Surely there are other options. But I didn't test other programmers.
Maybe you have to valid it by yourself.
This programmer for freescale DSC MCU comes from China, supporting MWCT family.
Ref: http://www.lunkedz.com/?/goods/id-14/index.html
Hi,
I mean a ICSP (in circuit system programmer) to download the firmware in the internal flash without using a bootloader or to write the bootloader.
For example, Microchip has a ICD3 or PICKit3 MPLAB ICD 4 In-Circuit Debugger
ATMEL has one too Atmel-ICE