Hello,
THe customer is using the PCF85063ATL/1,118.
Can you help provide the difference between these two parts based on the 2nd line changing from 0118 to 0210 on the part markings? I believe they are rev levels as there is only one way to order these parts from distribution.
063A versus 063A
0118 0210
*134 *207
(*) being the NXP logo.
What would be the differences in these two parts as the board LEDs are behaving differently using the chips programmed with the same FW level.
Regards,
David B.
Hello David,
I can support you for technical issues of our component. Could you please describe what is the issue with the PCF85063A? The PCF85063A is an RTC (Real Time Clock) component. It is not a LED driver. Could you please clarify the statement: "the board LEDs are behaving differently"
Please share your schematic with voltage levels and part values.
Regarding the top marking, I do not have access to decoding information.
With Best Regards,
Jozef