PCF85063ATL/1,118 Part Markings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF85063ATL/1,118 Part Markings

260 Views
DavidB4700
Contributor I

Hello, 

THe customer is using the PCF85063ATL/1,118. 

Can you help provide the difference between these two parts based on the 2nd line changing from 0118 to 0210 on the part markings?     I believe they are rev levels as there is only one way to order these parts from distribution.

063A      versus      063A

0118                       0210

*134                       *207

(*) being the NXP logo.

What would be the differences in these two parts as the board LEDs are behaving differently using the chips programmed with the same FW level. 

Regards, 

David B. 

0 Kudos
Reply
2 Replies

228 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello David,

I can support you for technical issues of our component. Could you please describe what is the issue with the PCF85063A? The PCF85063A is an RTC (Real Time Clock) component. It is not a LED driver. Could you please clarify the statement: "the board LEDs are behaving differently"

Please share your schematic with voltage levels and part values. 

Regarding the top marking, I do not have access to decoding information.

With Best Regards,

Jozef

0 Kudos
Reply

236 Views
Veronika_techsupport
NXP TechSupport
NXP TechSupport

Hello @DavidB4700 

please find the reply in the separate email.

Regards

0 Kudos
Reply