PCF2127 and TS pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF2127 and TS pin

1,247件の閲覧回数
ivekengineer
Contributor III

What should the voltage be on the TS pin (unconnected to any external devices) relative to either VBAT or VDD?  Should it be any different with TSOFF = 0 vs. TSOFF = 1?

On my board, when VBAT is ~2.5V I am measuring ~2.0V on my TS pin.  This would imply that either I'm leaking 2.5uA through the 200k pull-up resistor, or there is a diode from VBAT to one leg of the internal 200k pull-up resistor.  I would like to make sure I'm  not leaking 2.5uA as that would significantly reduce my supercap hold-up time.

タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,173件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

I tested in EVB with Vbat@3.2V and Ts@3.15V,so the leakage current is about 0.3uA.

0 件の賞賛
返信

1,173件の閲覧回数
ivekengineer
Contributor III

Was that with a setting of TSOFF = 0 or TSOFF = 1?  Would that even make a difference?

0 件の賞賛
返信

1,173件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

This is decided by open drain structure,I don't think they are difference when the bit set or not!

0 件の賞賛
返信

1,173件の閲覧回数
ivekengineer
Contributor III

That's what I would expect but I wanted to make sure.  Thanks!

BTW, I suspect my DMM has a low input impedance and that is why I'm seeing a larger voltage drop on my TS pin vs. yours.

0 件の賞賛
返信