What should the voltage be on the TS pin (unconnected to any external devices) relative to either VBAT or VDD? Should it be any different with TSOFF = 0 vs. TSOFF = 1?
On my board, when VBAT is ~2.5V I am measuring ~2.0V on my TS pin. This would imply that either I'm leaking 2.5uA through the 200k pull-up resistor, or there is a diode from VBAT to one leg of the internal 200k pull-up resistor. I would like to make sure I'm not leaking 2.5uA as that would significantly reduce my supercap hold-up time.