PCAL6524 Libbary file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCAL6524 Libbary file

813件の閲覧回数
MRD3326
Contributor I

Hello,

I am working on PCAL6524.I am interfacing it with STM32h7.I need the library file of that, can you please provide me library.

タグ(1)
0 件の賞賛
4 返答(返信)

792件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

what kind of library do you need?

 

 

0 件の賞賛

751件の閲覧回数
MRD3326
Contributor I

I have to interface with stm32.For arduino board the library is available that kind of liberty I need for stm32.

0 件の賞賛

790件の閲覧回数
MRD3326
Contributor I

I have configure with it stm32.I need to read the voltage of 15v which are connected to one port pin. So how can access that register. They provide Linux driver or ardiuio libarary. That kind of libabry I need so I can read the register. 

0 件の賞賛

791件の閲覧回数
MRD3326
Contributor I

I have configure with it stm32.I need to read the voltage of 15v which are connected to one port pin. So how can access that register. They provide Linux driver or ardiuio libarary. That kind of libabry I need so I can read the register. 

0 件の賞賛