PCA9698BS Device Addressing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9698BS Device Addressing

ソリューションへジャンプ
1,641件の閲覧回数
ryan_smith
Contributor I

Hi,

I am utilizing the PCA9698BS I/O Expander in a design. For this part's device address I have the external strapping setup for address 0x20. But when I try to talk to address 0x20 over the I2C bus, I detect no I2C bus devices. But I actually detect the I/O Expander I2C bus on address 0x10. When I write commands to this address I am able to fully communicate with the PCA9698BS device. Why does the datasheet specify that the address is 0x20 (for the external strapping that I'm using), when address 0x10 works instead?? The device address 0x10 isn't even an option within the PCA9698BS datasheet.

Thanks,

Ryan

0 件の賞賛
返信
1 解決策
1,623件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2 返答(返信)
1,599件の閲覧回数
ryan_smith
Contributor I

Hi Erika,

Thanks for sharing this post. It was my assumption that something such as bit shifting was happening. Thanks for confirming.

-Ryan

0 件の賞賛
返信
1,624件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信