PCA9685PW/Q900 - Frequency measurement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9685PW/Q900 - Frequency measurement

303件の閲覧回数
gopalakrishna
Contributor I

In one of application, the Part No : PCA9685PW/Q900 using as a PWM generator and interfaced with processor over i2C lines.

Internal clock is used.

It is observed that, the PWM O/P frequency is not matching with configured values, here is the details,

  1. Pre-scale Frequency 24 Hz and measured 29 Hz

  2. Pre-scale Frequency 678Hz and measured 690 Hz

  3. Pre-scale Frequency 1524 Hz and measured 1553 Hz

Please let me know solution to fix this issue.

gopalakrishna_0-1707407382389.png

 

0 件の賞賛
返信
1 返信

293件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello, 

Please find below the answer from the Application engineer:

The PCA9685 is over ten years old and unfortunately all designers are gone. I can recall about this oscillator is untrimmed, so it is +/-25% variation.

We apologize for any inconvenience this may cause you.

0 件の賞賛
返信