PCA9306 allow 1.05V translation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9306 allow 1.05V translation?

275 Views
ShuKhan
Contributor I

Hi

From PCA9306 datasheet, the operation for Vref1 is 1.0V to 3.6V.

However, there is another paragraph stating the allows voltage level translation which does not include 1.05V and 1.1V.

Can the part translate 1.05V -> 2.5V/3.3V and 1.1V -> 2.5V/3.3V?

If no, can you recommend a suitable part for I2C bus translation? Thanks.

0 Kudos
Reply
1 Reply

259 Views
guoweisun
NXP TechSupport
NXP TechSupport

Has replied to you by your ticket.

0 Kudos
Reply