PCA9306 allow 1.05V translation?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCA9306 allow 1.05V translation?

227 次查看
ShuKhan
Contributor I

Hi

From PCA9306 datasheet, the operation for Vref1 is 1.0V to 3.6V.

However, there is another paragraph stating the allows voltage level translation which does not include 1.05V and 1.1V.

Can the part translate 1.05V -> 2.5V/3.3V and 1.1V -> 2.5V/3.3V?

If no, can you recommend a suitable part for I2C bus translation? Thanks.

0 项奖励
回复
1 回复

211 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Has replied to you by your ticket.

0 项奖励
回复