Hello every one,
I used S32DS IDE to create SKEAZ64 application project, and select KEAZ128 SDK, after the project is created, I can not see Processor Expert tool, whether the skeaz64 is not supported by Processor Expert? thanks!
Hi
KEA SDK does not support Processor Expert, so you can not see it.
Please refer the examples in FRDM-KEAZ Freedom Evaluation Board – QSP(FRDM-KEA-QSP\Quick Start Package v8\Code Project Examples and Sample Drivers (Evaluation Grade Only)\FRDM-KEAZ64\Driver Test SW for KEAZ64\Driver Test SW for KEAZ64)
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------