we find that when SPI CLK has 507.5mV,the watch dog can not start.
How low must the watch dog start in UJA1078?
You can understand that Vhys means the difference of switching threshold value between the input voltage increase and decrease.
Yes,according to the calculation,the switching threshold voltage is 0.6V(Vv1 = 5V), the value I measured is 0.5V,why is it considered to have a singal and no trigger watch dog?
Follow below picture connection:
Refer to below picture:
I'm sorry to bother you.
Whether the pull-down resistance on the SCK&SCSN is required?
No, because to ensure that the SCSN pin and the SCK pin are always on a defined level the SBC
contains an internal pull-up resistor to V1 at SCSN and an internal pull-down resistor to
GND at SCK
Vv1 = 5V -> Vth 1.5V~3.5V, minus Vhys -> min vaule is 0.6V,
Tha value I tested was 0.5V,which theoretically should not be consided singal,can you take a look at it?
Use a minimum of 0.3*2.97 = 0.891V > 0.5075V,
so in theory watch dog should be start?
I have asked my guest to check the resistance. Is there any other place to check?
what's your actual V1 value in your schematic?
The multimeter measured 5V.
The threshold should be 1.5V min, 0.5V can't be considered valid value.
The result was that 0.5V did not trigger watch dog.
How can I slove this problem or are there any experiments I can try?
If you want to trigger this threshold which need at lease 1.5V ,so 0.5V can't trigger it which make sense.
OK, at UJA1078,how low is the single level on SPI enough to trigger watch dog?
should be as 0.3*V1 to 0.7*V1
If SPI doesn't have a communication,it won't feed the dog so ic will reset.
The results of our experiment that SPI CLK measure 0.5V,but ic not reset.
Will the IC reset in the following range?
0~0.3V1
0.3~0.7V1
0.7~V1
should be 0.3-0.7 V1 and above 0.7V1