Needed USBOTG driver to act as Device port on MCIMX31

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Needed USBOTG driver to act as Device port on MCIMX31

跳至解决方案
1,743 次查看
sac
Contributor I
Hi,
 Is  there any basic driver frame work or uboot code for for OTG port on MCIMX31 .So that it can brought up before falshing any thing. Basically I am looking for UMON driver which can bring up OTG port as device port
0 项奖励
回复
1 解答
1,016 次查看
Voxan
Contributor III
Hi Sac,

you may want to check at the following URL:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A7

click the 'i' button to get an overview of the BSP supported feature. If you download that BSP you'll get more complete information on available drivers...

Hope this helps...

Best Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,017 次查看
Voxan
Contributor III
Hi Sac,

you may want to check at the following URL:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A7

click the 'i' button to get an overview of the BSP supported feature. If you download that BSP you'll get more complete information on available drivers...

Hope this helps...

Best Regards
0 项奖励
回复