Needed USBOTG driver to act as Device port on MCIMX31

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Needed USBOTG driver to act as Device port on MCIMX31

Jump to solution
1,740 Views
sac
Contributor I
Hi,
 Is  there any basic driver frame work or uboot code for for OTG port on MCIMX31 .So that it can brought up before falshing any thing. Basically I am looking for UMON driver which can bring up OTG port as device port
0 Kudos
Reply
1 Solution
1,013 Views
Voxan
Contributor III
Hi Sac,

you may want to check at the following URL:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A7

click the 'i' button to get an overview of the BSP supported feature. If you download that BSP you'll get more complete information on available drivers...

Hope this helps...

Best Regards

View solution in original post

0 Kudos
Reply
1 Reply
1,014 Views
Voxan
Contributor III
Hi Sac,

you may want to check at the following URL:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061033202A7

click the 'i' button to get an overview of the BSP supported feature. If you download that BSP you'll get more complete information on available drivers...

Hope this helps...

Best Regards
0 Kudos
Reply