Matching network for MMG20241H

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Matching network for MMG20241H

744件の閲覧回数
stefanomoscato
Contributor I

Dear all, I will embed the MMG20241H wideband driver in an RF high power board for LTE communications. I have issues to reproduce with the circuit simulator the EVB matching network for 1700-2100 MHz band.

I used the S2P parameter, the transmission lines are well dimensioned (as datasheet reports) and also the substrate set is the same of the EVB.

Do you have any suggestions?

Thanks in advance for your priceless time!

Stefano

ラベル(1)
  • RF

タグ(2)
0 件の賞賛
1 返信

641件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Please create a Service request for this issue.

How I could create a Service Request?

0 件の賞賛