In order to clarify our status for regulatory compliance, I would like to receive confirmation that the product derived from Marvell 88MW300 QFN-68 is a non-adaptive equipment under EN 300 328 V2.2.2. To be more specific, related product is Azurewave AW-CU300 IEEE 802.11 b/g/n WLAN Microcontroller Module:
EN 300 328 V2.2.2 info
Thank you in advance.
解決済! 解決策の投稿を見る。
Hi,
here is the document , you can download it from nxp website.
https://www.nxp.com.cn/docs/en/application-note/AN12910.pdf
Have a good day!
Regards,
weidong
Hi,
here is the document , you can download it from nxp website.
https://www.nxp.com.cn/docs/en/application-note/AN12910.pdf
Have a good day!
Regards,
weidong
Hi,
See below, plese!
So it is an adaptive device.
Have a good day!
Regards,
weidong
To whom it may concern:
For your information, we are currently manufacturing Wi-Fi Adapter with Azurewave AW-CU300 Wi-Fi module based on Marvell 88MW300.
We are now planning to carry out RED certification testing in Europe and would like to check availability of a SW tool to manually set the Wi-Fi channel, bandwidth, bit rate, etc. as part of this RED testing for Wi-Fi Adapter.
Your feedback is appreciated. Thank you.
Hello Weidong:
Thank you for your reply.
If possible, could you please help be more specific about your reasoning? Based on which specific information from the Marvell product datasheet were you able to make this judgment that it is adaptive instead of non-adaptive? Thank you in advance.