Is anyone using the MC12311 successfully? We cannot receive valid packets at all. Transmitter is sending complete packets and receiver RSSI responds correctly. SyncAddressMatch and correct CRC are never set. Receiver RegOpMode is fixed at $10 but the IRQ flags show RxReady toggling on and off. Should it keep switching on and off like that even when there is no mode switching?
解決済! 解決策の投稿を見る。
Most of these "bugs" have a simple solution and so did this one. It needed just a couple of bytes in the right place.
I am... at least so far.
I have two MC12311 evaluation boards and am able to make them communicate flawlessly. My end goal, however, is to use one of them in a TPMS system with an FXTH87 transmitting and I'm still working on some technical hurdles.
p.s. I do realize this is an old thread but my experiences are current and hopefully a reply here will initiate more discussion.
Most of these "bugs" have a simple solution and so did this one. It needed just a couple of bytes in the right place.