MC12311 use

cancel
Showing results for 
Search instead for 
Did you mean: 

MC12311 use

Jump to solution
495 Views
steveh
Contributor II

Is anyone using the MC12311 successfully?  We cannot receive valid packets at all.  Transmitter is sending complete packets and receiver RSSI responds correctly.  SyncAddressMatch and correct CRC are never set.  Receiver RegOpMode is fixed at $10 but the IRQ flags show RxReady toggling on and off.  Should it keep switching on and off like that even when there is no mode switching?

0 Kudos
1 Solution
259 Views
steveh
Contributor II

Most of these "bugs" have a simple solution and so did this one.  It needed just a couple of bytes in the right place.

 

 

View solution in original post

0 Kudos
3 Replies
259 Views
georgepeterson
Contributor II

I am... at least so far.

I have two MC12311 evaluation boards and am able to make them communicate flawlessly. My end goal, however, is to use one of them in a TPMS system with an FXTH87 transmitting and I'm still working on some technical hurdles.

0 Kudos
259 Views
georgepeterson
Contributor II

p.s. I do realize this is an old thread but my experiences are current and hopefully a reply here will initiate more discussion.

0 Kudos
260 Views
steveh
Contributor II

Most of these "bugs" have a simple solution and so did this one.  It needed just a couple of bytes in the right place.

 

 

0 Kudos