Losing control over pwm channels on pca9685 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Losing control over pwm channels on pca9685 chip

801 Views
chasen
Contributor I

Hi,

I'm working with a pca9685 16-channel, 12-bit PWM I2C-bus LED controller. It's being used to control 12 volt relays (link below). I'm having a weird issue where I lose control of individual channels during testing. A channel will get stuck either high or low and requires a board reset in order to regain control. The board I'm using is from ncd(link below) and should be able to handle the relay load. Any feedback or advice would be greatly appreciated. 

Thank you,

Relay: Ice Cube Control Relay: 15A, SPDT, socket mount (PN# 781-1C-12D) | AutomationDirect 

board: PCA9685 16-Channel 8W 12V FET Driver Proportional Valve Controller with I2C Interface - store.ncd.io 

0 Kudos
3 Replies

228 Views
Ben-Michel
Contributor I

Did you solve the issue?
We got a similar problem here.

0 Kudos

757 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you mind share your schematic?

0 Kudos

464 Views
SmartCcy
Contributor I

你好,我也碰到了这个问题。PCA9685使用一段时间后,发现有引脚无法进行控制了

0 Kudos