Hi I m using LS1028A Processor for my project. I want more clarifications on JTAG Interface for LS1028A. I was referring to the document named "QorIQ LS1028A Design Checklist" to know about Jtag Interface requirement. In pg-54 of the document, they have shown a logic gate circuit for "TRST_B". Can u please elaborate the circuit in terms of the dependent variables for the jtag access and in terms of timing requirement?
The logic gate, it is to avoid when you are performing a POR reset, that the device get the TRST signal of the JTAG. If you are not planning to use the POR_B signal you can dismiss the usage of the logical gate.
Hi @jamesbone
I have few queries regarding same topic -:
1) TRST_B signal has a timing requirement as stated by Processor's datasheet as shown below. Who shall provide TRST_B with the given timing?
2) Is there any timing relation between PORESET_B and TRST_B ?
3) If we have an option to dismiss the usage of the logical gate, where shall the nRESET from Codewarrior to be connected ?