Is TFA9879 suitable for 8bit mono 22.05kHz I2S ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is TFA9879 suitable for 8bit mono 22.05kHz I2S ?

805 Views
aloysetech
Contributor I

Hi,

I'm note familiar with I2S and I'm looking for an I2S amplifier for the following audio format : 8bit mono at 22050Hz.

I found the TFA9879, but I'm not sure if it could work with my setup. Any information is appreciated.

Thanks,

Theo Meyer

0 Kudos
Reply
1 Reply

738 Views
darioarias
NXP Employee
NXP Employee

Hi Theo,

The TFA9879 is compatible with your set up because it does have a I2S digital input,  and it does support audio format 8-bit at 22.05kHz. What is the part you are not sure about?

Darío

0 Kudos
Reply