Hi,
I'm note familiar with I2S and I'm looking for an I2S amplifier for the following audio format : 8bit mono at 22050Hz.
I found the TFA9879, but I'm not sure if it could work with my setup. Any information is appreciated.
Thanks,
Theo Meyer
Hi Theo,
The TFA9879 is compatible with your set up because it does have a I2S digital input, and it does support audio format 8-bit at 22.05kHz. What is the part you are not sure about?
Darío