Hi, this is Bob.
I would like to know if TDF8546ATH/N1ZJ is replaceable with TDF8546TH/N2Z.
is it okay to apply TDF8546ATH/N1ZJ?
according to the datasheet, it says redesign. Please help confirm.
original usage : TDF8546TH/N2Z
NEW SUGGESTION : TDF8546ATH/N1ZJ
+ Can I know what is N1 / N2 / Z meaning?
I think Z / J means T&R. can you check is this right?
thank you so much in advance.
Best regards,
Solved! Go to Solution.
Hello Bob,
https://www.nxp.com/part/TDF8546TH#/
J means plastic DIL-bent-SIL (special bent) power package; 27 leads (lead length 6.8 mm) = SOT827-1
N1Z or N2Z is the fab differentiator
The TDF8546A is a redesign of the TDF8546 having a lower quiescent current and improved electromagnetic immunity (EMI) properties. The TDF8546 and TDF8546A use an asymmetrical input configuration, delivers 25 W of output power, and is available in several bend variants of DBS27 or HSOP36 package.
Please refer to: https://www.nxp.com/docs/en/brochure/75017414.pdf
Best regards
Pavla
Hello Bob,
https://www.nxp.com/part/TDF8546TH#/
J means plastic DIL-bent-SIL (special bent) power package; 27 leads (lead length 6.8 mm) = SOT827-1
N1Z or N2Z is the fab differentiator
The TDF8546A is a redesign of the TDF8546 having a lower quiescent current and improved electromagnetic immunity (EMI) properties. The TDF8546 and TDF8546A use an asymmetrical input configuration, delivers 25 W of output power, and is available in several bend variants of DBS27 or HSOP36 package.
Please refer to: https://www.nxp.com/docs/en/brochure/75017414.pdf
Best regards
Pavla
Dear Pavla,
thank you for the kind reply.
can you also check what is Z stands for?
TDF8546TH/N2Z