Is SGTL5000XNBA3 a drop-in replacement for SGTL5000XNAA3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is SGTL5000XNBA3 a drop-in replacement for SGTL5000XNAA3?

ソリューションへジャンプ
685件の閲覧回数
DanKSI
Contributor III

Hi,

I have an existing design using a SGTL5000XNAA3, which is now obsolete.  I see there is the SGTL5000XNBA3, which has the same pinout.  Would switching to the "B" part require a board re-spin or is this a drop-in replacement?

Thanks,

Dan K.

タグ(1)
0 件の賞賛
返信
1 解決策
662件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dan,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the SGTL5000XNAA3 device is obsolete.

In this case, you may use the SGTL5000XNBA3 device as a direct replacement.

Please be aware that there is a slight difference between the packages. You may review the package dimensions from the datasheet.

diazmarin09_0-1686334645315.png

 

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

2 返答(返信)
652件の閲覧回数
DanKSI
Contributor III

That is the exact info I was looking for.

Thanks,

Dan K.

0 件の賞賛
返信
663件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Dan,

I hope all is great with you. Thank you for using the NXP communities.

You are correct, the SGTL5000XNAA3 device is obsolete.

In this case, you may use the SGTL5000XNBA3 device as a direct replacement.

Please be aware that there is a slight difference between the packages. You may review the package dimensions from the datasheet.

diazmarin09_0-1686334645315.png

 

I hope this information helps.

Regards,

David