Hello,
I'm using NXP-SC16IS750 as I2C to UART bridge in Linux embedded board with kernel 4.4.120, but both of the RS232 /RS485 are not working.
Attach is the SC16IS7xx driver that we used.
The /dev/ttySC0 shows up after modifying the DTS to fit our hardware design.
The test result fails when an X86 PC connects to this embedded board (w/ SCI16IS750).
The test result is okay if the X86 PC connects to another board.
The scope connects to the PC side, which shows the DB9 TX pin has the signal when the PC side sends some characters.
No signal shows up on DB9 TX and RX pins, when this embedded board sents some characters.
Is there specific item that we need to implement or which driver should we used to implement the function of SC16IS750 bridge?
DTS
i2c@11000 {
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
status = "okay";
clock-frequency = <100000>;
sc16is750: sc16is750@48 {
compatible = "nxp,sc16is750";
interrupts-extended = <&gpio0 11 8>;
clocks = <&coreclk 0>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
reg = <0x48>;
};
};
Thanks.
Hi both,
Any news on the driver provided by JozefKozon? I'm experiencing issues with the Linux included driver (kernel 5.4.148)
sc16is7xx.c - drivers/tty/serial/sc16is7xx.c - Linux source code (v5.4.148) - Bootlin
The driver seems to build successfully and I'm able to read/write registers to the sc16is750 with "i2cget/i2cset" commands but the driver doesn't take over the device
Tried this
And this in the DTS
Hi All,
please see below an answer from an application engineer regarding the Linux driver for SC16IS750.
I apologize for inconvenience.
DESCRIPTION
We do not provide any support for the Linux driver since we don’t have a software engineer. Years ago we offered a Linux driver for kernel as reference. The customer could use the driver as is, as their own risk. We did not offer any software support and it is still the same.
With Best Regards,
Jozef