How to enable-disable local bus cache on MPC8347

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to enable-disable local bus cache on MPC8347

跳至解决方案
1,920 次查看
Nachiketas
Contributor I
Hello,
Is it possible to programmatically enable-disable local bus cache on MPC8347?
Is it possible to check programmatically whether the local bus cache on MPC8347 is enabled?
I will appreciate any help, including a reference to the appropriate documentation.
Regards,
N
0 项奖励
回复
1 解答
905 次查看
genuap
NXP Employee
NXP Employee
Do you want to disable caching of just the local bus (i.e. let the system still cache the DDR)? If so, then you need to modify your MMU settings (32-bit programming environments manual) and set the cache-inhibited option.

 ... Paul

在原帖中查看解决方案

0 项奖励
回复
2 回复数
905 次查看
Nachiketas
Contributor I
Thank you, Paul.
N
0 项奖励
回复
906 次查看
genuap
NXP Employee
NXP Employee
Do you want to disable caching of just the local bus (i.e. let the system still cache the DDR)? If so, then you need to modify your MMU settings (32-bit programming environments manual) and set the cache-inhibited option.

 ... Paul

0 项奖励
回复