How to enable-disable local bus cache on MPC8347

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable-disable local bus cache on MPC8347

Jump to solution
1,867 Views
Nachiketas
Contributor I
Hello,
Is it possible to programmatically enable-disable local bus cache on MPC8347?
Is it possible to check programmatically whether the local bus cache on MPC8347 is enabled?
I will appreciate any help, including a reference to the appropriate documentation.
Regards,
N
0 Kudos
Reply
1 Solution
852 Views
genuap
NXP Employee
NXP Employee
Do you want to disable caching of just the local bus (i.e. let the system still cache the DDR)? If so, then you need to modify your MMU settings (32-bit programming environments manual) and set the cache-inhibited option.

 ... Paul

View solution in original post

0 Kudos
Reply
2 Replies
852 Views
Nachiketas
Contributor I
Thank you, Paul.
N
0 Kudos
Reply
853 Views
genuap
NXP Employee
NXP Employee
Do you want to disable caching of just the local bus (i.e. let the system still cache the DDR)? If so, then you need to modify your MMU settings (32-bit programming environments manual) and set the cache-inhibited option.

 ... Paul

0 Kudos
Reply