Firmware for SJA1105 Tool on LS1021ATSN-PA platform is missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Firmware for SJA1105 Tool on LS1021ATSN-PA platform is missing

跳至解决方案
158 次查看
Frank_Die
Contributor I

Hi out there,

currently im working on the LS10121ATSN-PA platform - installed with OpenIL. But after first steps with SJA1105 Tool to change switch configuration i get the error "could not open /lib/firmware/sja1105.bin for write". Where can i get the firmware?

 

Greetings Frank

0 项奖励
回复
1 解答
131 次查看
Frank_Die
Contributor I

I found a solution by myself. I used the offical Image OpenIL which contains the firmware for the SJA1105.

在原帖中查看解决方案

0 项奖励
回复
1 回复
132 次查看
Frank_Die
Contributor I

I found a solution by myself. I used the offical Image OpenIL which contains the firmware for the SJA1105.

0 项奖励
回复