Firmware for SJA1105 Tool on LS1021ATSN-PA platform is missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware for SJA1105 Tool on LS1021ATSN-PA platform is missing

Jump to solution
251 Views
Frank_Die
Contributor I

Hi out there,

currently im working on the LS10121ATSN-PA platform - installed with OpenIL. But after first steps with SJA1105 Tool to change switch configuration i get the error "could not open /lib/firmware/sja1105.bin for write". Where can i get the firmware?

 

Greetings Frank

0 Kudos
Reply
1 Solution
224 Views
Frank_Die
Contributor I

I found a solution by myself. I used the offical Image OpenIL which contains the firmware for the SJA1105.

View solution in original post

0 Kudos
Reply
1 Reply
225 Views
Frank_Die
Contributor I

I found a solution by myself. I used the offical Image OpenIL which contains the firmware for the SJA1105.

0 Kudos
Reply