Firmware for SJA1105 Tool on LS1021ATSN-PA platform is missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware for SJA1105 Tool on LS1021ATSN-PA platform is missing

ソリューションへジャンプ
144件の閲覧回数
Frank_Die
Contributor I

Hi out there,

currently im working on the LS10121ATSN-PA platform - installed with OpenIL. But after first steps with SJA1105 Tool to change switch configuration i get the error "could not open /lib/firmware/sja1105.bin for write". Where can i get the firmware?

 

Greetings Frank

0 件の賞賛
返信
1 解決策
117件の閲覧回数
Frank_Die
Contributor I

I found a solution by myself. I used the offical Image OpenIL which contains the firmware for the SJA1105.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
118件の閲覧回数
Frank_Die
Contributor I

I found a solution by myself. I used the offical Image OpenIL which contains the firmware for the SJA1105.

0 件の賞賛
返信