FIT / MTTF data for TJA1051T/3,118

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FIT / MTTF data for TJA1051T/3,118

1,078 Views
rowangifford
Contributor II

Hello,

Where can I find FIT / MTTF data for TJA1051T/3,118?

IC markings:

A150 1/3

B706

nD914

Thanks,

Rowan

Tags (3)
0 Kudos
Reply
1 Reply

983 Views
Beckywang
NXP TechSupport
NXP TechSupport

Hello Rowan

Kindly refer to below information

Based upon life 
testing, in the amounts as prescribed by AEC-Q100, with 0 failures found, we 
can calculate a failure rate <10FIT, with 60% Confidence Level, at a 
junction temperature of 55°C with an activation energy of 0.7eV.  This 
failure rate equals an MTBF > 100M hours. These figures are sample size 
limited. 

Based upon 
justified field returns, so excluding EOS/ESD and NTF, we can calculate an 
experienced field failure rate << 1FIT. For this calculation we assume 
1.5 hours of operation per day, for each delivered product, this equals a 
typical automotive profile.

Have a great day,
Becky

 

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply