Hi All,
I made an nfc antenna for PN7150 with a design like the picture below. Performed testing obtained electromagnetic wave range of 1.34V. While the conditions that must be met is 6V. What do I need to change to meet these requirements?
Thank you,
Iwan
Hello,
In order to better service for you. Would you please describe how to test "electromagnetic wave range of 1.34V" ?
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
sorry i am wrong, that's the value of the strength of the electromagnetic field not "electromagnetic wave range".
tested using ISO/IEC10373-6, where the value of Hmin must be greater than 6V.
I don't really understand this.
Hello,
Thanks for your update information. For more information you can refer to the document as the link.
URL:https://www.nxp.com/docs/en/application-note/AN11755.pdf.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hello,
You are welcome.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------