Portability of NXP thread for K32W

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Portability of NXP thread for K32W

630 Views
sd05
Contributor III

Hello Community,

I had this doubt may be a stupid one but want to clear that if the NXP thread available with KW41Z SDK the lib

SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_br_cm0.a
SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_cm0.a
SDK_2.2.0_FRDM-KW41Z_LINUX/middleware/wireless/nwk_ip_1.2.6/core/lib/thread/lib_thread_ed_cm0.a

are platform specific?
As we have openthread which has a abstraction is it same with NXP thread?

Also where I can get NXP Thread stack source as what i can find are library?
Thanks!!

Tags (1)
0 Kudos
Reply
1 Reply

596 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. The files available for KW41Z are the ones you have in the SDK.

For K32W, you should use the OpenThread Stack available in the SDK and here: https://github.com/openthread/ot-nxp

 

Regards,

Ricardo

0 Kudos
Reply