Electrical Field PN7150 Antenna Design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Electrical Field PN7150 Antenna Design

1,206件の閲覧回数
iwannugraha
Contributor III

Hi All,

I made an nfc antenna for PN7150 with a design like the picture below. Performed testing obtained electromagnetic wave range of 1.34V. While the conditions that must be met is 6V. What do I need to change to meet these requirements?

My antenna design for PN7150My antenna design for PN7150

 

Thank you,

 

Iwan

ラベル(1)
  • RF

タグ(2)
0 件の賞賛
5 返答(返信)

1,186件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

In order to better service for you. Would you please describe how to test  "electromagnetic wave range of 1.34V" ?

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛

1,176件の閲覧回数
iwannugraha
Contributor III

sorry i am wrong, that's the value of the strength of the electromagnetic field not "electromagnetic wave range".
tested using ISO/IEC10373-6, where the value of Hmin must be greater than 6V.
I don't really understand this.

0 件の賞賛

1,153件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your update information. For more information you can refer to the document as the link.

URL:https://www.nxp.com/docs/en/application-note/AN11755.pdf.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

1,149件の閲覧回数
iwannugraha
Contributor III

Hi,

 

Thank you for your information. i will follow the document and inform you.

0 件の賞賛

1,106件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

You are welcome.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------