EP8248

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EP8248

1,974 次查看
muralee
Contributor I
Hi,
      I am new to linux. I have to port linux-2.6 to MPC8248 processor board (EP8248).  What i have is,
       1)  EP8248 Board
       2)  MPC8272ADS BSP
       3)  Code warrior USB TAP Emulator

Can any one tell me, can i use this bsp for EP8248 board.

Also,
I tried downloading the sample images given in the BSP. But After the message "
Uncompressing Kernel Image ... OK" its hanging. Can you please help


U-Boot 1.0.0 (Feb 22 2006 - 16:14:27)

MPC8260 Reset Status: External Soft, External Hard

MPC8260 Clock Configuration
 - Bus-to-Core Mult 3.5x, VCO Div 2, 60x Bus Freq  30-100, Core Freq 100-400
 - dfbrg 1, corecnf 0x1e, busdf 3, cpmdf 1, plldf 0, pllmf 5
 - vco_out  396000000, scc_clk   99000000, brg_clk   24750000
 - cpu_clk  346500000, cpm_clk  198000000, bus_clk   99000000

CPU:   8272 (HiP7 Rev 14, Mask A.0 1K50M) at 346.500 MHz
Board: Embedded Planet EP8248, Revision 1.0
I2C:   ready
DRAM:  16 MB
FLASH:  8 MB
In:    serial
Out:   serial
Err:   serial
COntrol Reg - 3020
Status Reg - 7809
Auto Adver Reg - 1a1
Link Partner Reg - 0
Net:   FCC1 ETHERNET
Hit any key to stop autoboot:  0
## Booting image at fff20000 ...
   Image Name:   Linux-2.6.11-XXXXX
   Image Type:   PowerPC Linux Kernel Image (gzip compressed)
   Data Size:    568617 Bytes = 555.3 kB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
   Uncompressing Kernel Image ... OK

Thanks in ADVANCE.
Any nonsense plz forgive.
0 项奖励
回复
1 回复

900 次查看
PaoloTreffilett
Contributor II
Hi,
this seems a problem of your BSP. I have found the same problem using the BSP for the EP8548 version 1.1 with the EP8548 version 1.2, I had to use a new version of the BSP to work with a new version of the mezzanine.
I think that you must use the BSP for the EP8248 or build your own environment from scratch.

Best regards,
Paolo


Message Edited by Paolo Treffiletti on 2007-09-21 09:42 AM

Message Edited by Paolo Treffiletti on 2007-09-21 09:45 AM
0 项奖励
回复