Does DTM test use DTM rx or Uart?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does DTM test use DTM rx or Uart?

741 Views
jingfang
Contributor IV

If i want DTM test, can I  use 43 &44 ,only uart, or need use 46 &47 has DTM rx.企业微信截图_1675931633954.png企业微信截图_16759316798906.png

0 Kudos
Reply
3 Replies

730 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @jingfang ,

 

Hope you are doing well.

I think using DTM_TX and DTM_RX will be okay. 

For the operation of KW series boards for DMT, our colleagues have written a concise document. You can refer to this link: Direct Test Mode (DTM) Configurations for the KW family 

 

If you have problems accessing this document, please don't hesitate to let me know and I will resend it to you.

 

B.R.

Gavin

0 Kudos
Reply

728 Views
jingfang
Contributor IV

The document :

企业微信截图_16760198521774.png

So I think uart it is ok, but I/O show DTM RX/TX,so I'm a little confused.

0 Kudos
Reply

711 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @jingfang ,

There are two ways to realize DTM test, one is through HCI, the other is through 2-wire uart interface. The documentation mentioned above is based on the 2-wire uart interface for testing.

The drivers used by DTM_Rx and DTM_Tx are also UART drivers. But multiplexing the GPIOs directly as DTM_Rx and DTM_Tx for DTM testing will eliminate possible problems later, and I can't guarantee that multiplexing as uart_tx/rx will still work.

 

B.R.

Gavin

0 Kudos
Reply